Hi everyone, I'm looking to design and develop a USB Audio Interface using STM32F4xx series MCUs that could ideally record up to 16 channels of analog audio signals, convert and send to a PC / MAC via USB.
If anyone is familiar with Digital Audio Workstations (DAW's), you can then select the type of audio input device in the application, to then choose which channel to monitor and record.
I'm familiar with the process of how to record the incoming audio signals via the onboard STM ADC's however I'm not sure on how to the pass that converted digital audio using the USB protocol so that the computer can identify the audio interface, and be able to choose each channel.
Any help or recommended readings would be great.
Thanks :)