Hi i'm working on Nucleo-l073rz board to bring up sd card and fatfs using spi interface for data logging application.
I am testing the above setup using an transcend micro sd card adapter with 16GB sd card.I have no response from the sd card , i have used 32MHz clock with a spi baud rate 8MBits/s.i have used drivers from STM32Cube_FW_L0_V1.11.2\Drivers\BSP\Adafruit_Shield\stm32_adafruit_sd.c.I am not able to even mount the sd card .let me know what could be the problem is their any limitations ,thanks in advance.