Skip to main content
Visitor II
July 29, 2020
Question

How can the external ULPI USB transceiver chip (U4 - USB3320C) on the STM32H747I-DISCO board fail and cause a permanent short circuit?

  • July 29, 2020
  • 0 replies
  • 513 views

I tried to configure the MCU as a mass storage device using Cubemx without success. The board was connected to the computer with CN1 and CN2 at the same time.

I confirmed that the short was caused by U4 by removing it. After removal of U4 the current consumption dropped from +-1A to +-150 mA.

    This topic has been closed for replies.