How do I determine when Virtual Com Port is closed/opened in my STM32L476 firmware?
I'm working with the Nucleo-64 development board with an STM32L476 microcontroller and I'm using the USB source code that STM32CubeMX has generated for me. I want to be able to find out when the Virtual Com Port is closed/opened on the PC that the Nucleo-64 board is connected to. I've googled quite a bit, some suggests the condition is (Bool_t)(hUsbDeviceFS.ep0_state == USBD_EP0_STATUS_OUT), others suggest I should evaluate req->wValue inside the CDC_SET_CONTROL_LINE_STATE case statement in CDC_Control_FS. However, none of these methods work reliably for me. Can anybody please help me?