How do I put the original flash bootloader back onto a device if I've erased or corrupted it?
I'm not sure how I did it, but my Blue Pill STM32F103C8T6 doesn't respond to st-info --probe any more. This has happened twice in a row with identical devices. It seems that if I Ctrl-D out of GDB (an old bad habit) the device seems to brick itself and won't respond to programming or STLINK probes. I'm using an STLINK/V2 programmer attached to the SWIO/SWCLK pins.
I can still set the BOOT0 pin to boot the system ROM bootloader and get proper responses from the STLINK/V2 programmer. So, I'm wondering where I can download the original flash bootloader and what address I'd need to use with st-flash to flash it back onto the device so that I can return to a nice wholesome flash bootloader.