Skip to main content
Explorer II
March 2, 2022
Question

How download text file from browser to stm32h743 webserver

  • March 2, 2022
  • 0 replies
  • 459 views

I  have set up an STM32H743 nucleo webserver which works OK by presenting a small webpage on a browser (I am using LWIP+CubeIDE).

I can give the webserver simple commands via CGI (see below) and thereby print something to the serial port. Unfortunately, I cannot seem to find a way download a file from the browser to the webserver and onwards to the serial port of the STM32. I don't need to store this data, just pass it through to the port. I am not an expert as you can see, but could someone point me into the right direction as regards the simplest way to do this? I don't really want to add any more hardware. My colleague says this is not possible, but I dont see why not.

Thanks for any ideas!

const char * valueCGIhandler(int iIndex, int iNumParams, char *pcParam[], char *pcValue[])

{

uint32_t i=0;

if (iIndex == 0)

{

if( strstr((*pcParam),"SETPOINT"))

{

Println(&huart3,*pcValue);

}

}

return "/index.shtml";

}

    This topic has been closed for replies.