How should I implement the IAP (In-Application Programming) functionality on the STM32F745?
I want to implement a firmware upgrade feature. Currently, I am doing it as follows: on the M4 core, I have a bootloader and an application; on the M7 core, there is also a bootloader and an application. The M4 application is located at address 0x08120000, and the M7 application is located at address 0x08020000. I’m not sure if this approach is feasible or if there is a recommended upgrade method. Currently, the jump between the cores does not succeed, and I don’t know why. Are there any specific considerations when performing a jump between dual-core firmwares?