Skip to main content
Graduate
January 22, 2020
Question

How to add 2 HID devices ?

  • January 22, 2020
  • 2 replies
  • 785 views

In the demo for Keyboard or Mouse, its one or the other,

how can you run a Keyboard and a Mouse ?

    This topic has been closed for replies.

    2 replies

    Visitor II
    January 28, 2020

    mention part number ,

    Graduate
    January 28, 2020

    it is a H743 board

    the device "cap touch" is limping along on FS Host,

    luckily the touch chip responds with the data I need, so one finger is running

    but when I plug in the Keyboard HS host the touch dies but the keyboards works

    then unplug and nothing works, guess I should trap that and deinit/reinit

    Still unable to send a control packet to the touch chip, not sure how to. couldn't find an example.

    Could you point me to the description of "report type " or a usage example of this:

    1. USBH_StatusTypeDef USBH_HID_SetReport(USBH_HandleTypeDef *phost,
    2. uint8_t reportType,
    3. uint8_t reportId,
    4. uint8_t *reportBuff,
    5. uint8_t reportLen);