How to get rid of "float formatting support is not enabled" in STM32CubeIDE for CMake project
Hi Community,
I am working on a CMake project where sprintf is being used. After building the project in the Problems window section, I see one error regarding the float formatting as below.
The float formatting support is not enabled, check your MCU Settings from "Project Properties > C/C++ Build > Settings > Tool Settings", or add manually "-u _printf_float" in linker flags
The flag "-u _printf_float" is added in the target link options and -mfpu=fpv4-sp-d16 and -mfloat-abi=hard is added as CPU parameters. But still showing this problem will it impose any issue while building although the build is not complaining about this.