How to get the B-L462E-CELL1 cellular MQTT example working?
I downloaded the en.x-cube-cellular.zip and unziped the folder STM32CubeExpansion_CELLULAR_V5.2.0. I then installed the changes to upgrade to V5.2.1.
I imported the project into CubeIDE and found the MQTT sample was not imported. I then tried to follow the mqtt readme.txt where i have to "Remove 'Exclude from build' option for the following components of the IART project". That note is not too helpful because, as far as I can tell, there are no excluded files that I can include.
Anyone know how to get MQTT working for this DISCO board?