How to make the Nx_MQTT_Client (STM32Cube_FW_U5_V1.1.0) connect to AWS?
Hello - just trying to make a sanity connection to AWS IOT, unsecured port 1883, but it fails with a very non-specific error like not connected. I changed the demo app to use unsecure port 1883 and it connects and successfully sends the MQTT messages to the mosquito as well as the hivemq test server. But when I plug in my AWS IOT endpoint for MQTT_BROKER_NAME it does not connect. Any hints or tips or tricks?
On a side note, when I undefined the secure connect variables (NX_SECURE_ENABLE and NXD_MQTT_REQUIRE_TLS) there was a bit of work to do to make it compile (and thereby connect in unsecure mode). It was not a big deal, but it would be nice if it was already done for the sake of sanity for the MQTT / IOT newbie.