How to program a nucle boat (L053R8) using UART?
hey,
I went through all possible data sheets I could find did all the required things but my Nucleo still won’t be programmed with uart.
I have put boot0 on VDD pin next to it. For confirmation I also put PB2 (nboot1) on ground next to it.
I tried powering the nucleo through both the USB as well as an external supply (E5V) and switched to e5v.
I reset the controller to try programming.
I connected my Rx, Tx and Ground of my UART to usb (which I checked with the nucleo by programming a UART program through st link and it works)
I am using St flash which says there was no communication
and stm32 programmer says it timed out for the com port
i even checked that there was no read or write protection enabled and nboot1 option bits are correct by connecting to stm32 programmer through STlink
what am I missing?