Skip to main content
Graduate
January 22, 2024
Question

How to remove stm32mp135f-dk-a7-examples.dtb from yocto build?

  • January 22, 2024
  • 1 reply
  • 1098 views

I have two doubts kind clear it.

1) I want remove and dont want to build stm32mp135f-dk-a7-examples.dtb, so where can I remove example dtb which is selected from extlinux.conf?

2) I want to mount my desired partition where and how it can be mounted?

 

    This topic has been closed for replies.

    1 reply

    Visitor II
    January 22, 2024

    To remove the building of stm32mp135f-dk-a7-examples.dtb, you'll need to modify the configuration files. I think you'll get more helpful responses if you share more details.

    Graduate
    January 23, 2024

    Dear sir,

    1) If you see during boot, we have option to select different dtb like stm32mp13f-dk.dtb and stm32mp135f-dk-a7-examples.dtb. I just want my kernel should start with stm32mp13f-dk.dtb and there should not be any option to select any other dtb. But when building rootfs, this file comes automatically. I just want to remove all example dtb from yocto build so that it dont come in /boot folder of rootfs.

    2) I want to mount partition like user2.ext4 and vendor2.ext4 in my hardware, how is that possible using yocto build process?