How to run bootloader on bricked STM32H7 Discovery kit?
I have recently bricked my STM32H7 discovery kit by trying to select the M4-only boot option, but I am no longer able to connect the debugger. I have had a similar problem with the Arduino Giga board but I managed to "unbrick" it by running a bootloader and pressing the "BOOT0" button. According to the STM32H7 manual, the bootloader should is loaded by a combination of a high BOOT0 and the status of certain option bits (over which I obviously do not have any control any longer). For the Discovery board, I have soldered in a button that shorts out R192 and which I then press while powering up / resetting, but neither the STM32CubeProgrammer nor the ST flash loader demo is able to connect through the UART (via the in-built ST link programmer). Do you have any advice on how to start the bootloader? Surely there must be a way to save that board? Do I need to use a different USART port?
Many thanks,
Clem