How to send 16 bytes of data from USB keyboard(Using HID class ) to PC.I have sent 8 byte data it working properly. Unable to send 16 byte data.
I have done setting in Report descriptor as below,
0x05, 0x01, // USAGE_PAGE (Generic Desktop)
0x09, 0x06, // USAGE (Keyboard)
0xa1, 0x01, // COLLECTION (Application)
0x75, 0x01, // REPORT_SIZE (1)
0x95, 0x08, // REPORT_COUNT (8)
0x05, 0x07, // USAGE_PAGE (Keyboard)(Key Codes)
0x19, 0xe0, // USAGE_MINIMUM (Keyboard LeftControl)(224)
0x29, 0xe7, // USAGE_MAXIMUM (Keyboard Right GUI)(231)
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x01, // LOGICAL_MAXIMUM (1)
0x81, 0x02, // INPUT (Data,Var,Abs) ; Modifier byte
// 0x95, 0x01, // REPORT_COUNT (1)
0x95,0x10,
// 0x75, 0x08, // REPORT_SIZE (8)
0x75, 0x10,
0x81, 0x03, // INPUT (Cnst,Var,Abs) ; Reserved byte
0x95, 0x05, // REPORT_COUNT (5)
// 0x75, 0x01, // REPORT_SIZE (1)
0x75, 0x10,
0x05, 0x08, // USAGE_PAGE (LEDs)
0x19, 0x01, // USAGE_MINIMUM (Num Lock)
0x29, 0x05, // USAGE_MAXIMUM (Kana)
0x91, 0x02, // OUTPUT (Data,Var,Abs) ; LED report
0x95, 0x01, // REPORT_COUNT (1)
// 0x75, 0x03, // REPORT_SIZE (3)
0x75, 0x10,
0x91, 0x03, // OUTPUT (Cnst,Var,Abs) ; LED report padding
0x95, 0x06, // REPORT_COUNT (6)
// 0x75, 0x08, // REPORT_SIZE (8)
0x75, 0x10,
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x65, // LOGICAL_MAXIMUM (101)
0x05, 0x07, // USAGE_PAGE (Keyboard)(Key Codes)
0x19, 0x00, // USAGE_MINIMUM (Reserved (no event indicated))(0)
0x29, 0x65, // USAGE_MAXIMUM (Keyboard Application)(101)
0x81, 0x00, // INPUT (Data,Ary,Abs)
0xc0 // END_COLLECTION
HID.h file
#define HID_EPIN_ADDR 0x81U
#define HID_EPIN_SIZE 0x10 //0x08U
#define HID_EPOUT_ADDR 0x01
#define HID_EPOUT_SIZE 0x01
#define USB_HID_CONFIG_DESC_SIZ 34U
#define USB_HID_DESC_SIZ 16U //9U
#define HID_MOUSE_REPORT_DESC_SIZE 63U //74U
#define HID_DESCRIPTOR_TYPE 0x21U
#define HID_REPORT_DESC 0x22U
#ifndef HID_HS_BINTERVAL
#define HID_HS_BINTERVAL 0x07U
#endif /* HID_HS_BINTERVAL */
#ifndef HID_FS_BINTERVAL
#define HID_FS_BINTERVAL 0x0AU
#endif /* HID_FS_BINTERVAL */
#define HID_REQ_SET_PROTOCOL 0x0BU
#define HID_REQ_GET_PROTOCOL 0x03U
#define HID_REQ_SET_IDLE 0x0AU
#define HID_REQ_GET_IDLE 0x02U
#define HID_REQ_SET_REPORT 0x09U
#define HID_REQ_GET_REPORT 0x01U
HId.c file
0x03, /*bInterfaceClass: HID*/
0x00, /*bInterfaceSubClass : 1=BOOT, 0=no boot previously was 1*/
0x01, /*nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse*/