How to setup project for TouchGFX AND Audio Output
Hi All,
I want to start a project using TouchGFX, but it must also contain Audio Output on the headphone jack of my STM32F746G-DISCO board.
I managed to get these two things to work separately: The TouchGFX part using TouchGFX Designer, and the Audio Output using CubeIDE and an example project.
However, I cannot figure out how to get the sound output into my TouchGFX project! My approach is to call the appropriate BSP function (BSP_Audio_Out_Init / BSP_Audio_Out_Play) in the Model class of TouchGFX. Obviously, I need to include the necessary header files etc. - but that's where I run into problems. There are multiple dependencies so adding all manually is difficult and error-prone. And even if I manage to do all this, I'm getting compile/linker errors that I don't understand.
So my question is: Is there any automated way I can set up my project so I can use the Audio BSP functions from my TouchGFX code?