How to use fx_media_format and fx_media_open ?
Hello,
I am trying to set up FileX with USBX, but my computer recognizes a disk drive but does not see any volume.
Can you help me determine whether I am using the fx_media_format and fx_media_open functions correctly, given that they do not return any errors?
UINT ret = FX_SUCCESS;
/* USER CODE BEGIN MX_FileX_Init */
UINT RETT = lx_stm32_nor_custom_driver_initialize(&nor_flash);
/* USER CODE END MX_FileX_Init */
/* Initialize FileX. */
fx_system_initialize();
/* USER CODE BEGIN MX_FileX_Init 1*/
/* Format the NOR flash as FAT */
status = fx_media_format(&nor_flash_disk,
fx_stm32_levelx_nor_driver, // Driver entry
(VOID*)&nor_flash, // Device info pointer (VOID*)NOR_CUSTOM_DRIVER_ID
(UCHAR*)media_memory, // Media buffer pointer
sizeof(media_memory), // Media buffer size
"NOR_FLASH_DISK", // Volume Name
1, // Number of FATs
32, // Directory Entries
0, // Hidden sectors
TOTAL_SECTOR_LOGICAL, // Total sectors
SECTOR_SIZE_LOGICAL, // Sector size
8, // Sectors per cluster
1, // Heads
1); // Sectors per track
/* Check if the format status */
if (status != FX_SUCCESS)
{
Error_Handler();
}
/* Open the SPI NOR Flash disk driver. */
//status = fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver,(VOID*)NOR_CUSTOM_DRIVER_ID , media_memory, sizeof(media_memory));
status = fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver,(VOID*)NOR_CUSTOM_DRIVER_ID , media_buffer, sizeof(media_buffer));
/* Check the media open status. */
if (status != FX_SUCCESS)
{
Error_Handler();
}
For Device info pointer, should i use (VOID*)&nor_flash or (VOID*)NOR_CUSTOM_DRIVER_ID ?
Can the volume name and media name be different ?