How to use LPTIM with LSE source clock
Greetings,
I am using a Discovery Kit (B-U585I-IOT02A) and I want to use the LPTIM1 to wait 5 seconds (counting x ticks), at the end of the 5 seconds enter in a Callback to do something and then restart the counter again.I want to use as clock source the 32.768Khz crystal (LSE).
So, I configured the LSE clock in the RCC section of the .ioc, then I set the LSE as clock source for LPTIM1, and activated the interrupts.
At the main function, I used the HAL_LPTIM_TimeOut_Start_IT(&hlptim1, 16383) and used the void HAL_LPTIM_AutoReloadMatchCallback (LPTIM_HandleTypeDef* hlptim) callback to do something.
The callback is not being called, I measured the signal at the crystal, and I can't see any clock in it. I guess something's missing in the configuration but I have no clue what it is and I can't make it work.
An helping hand would be appreciated.