How to use the mutex RTOS .
Hi,
I want to synchronize the my threads execution using the mutex.
here is my code
/*----------------------------------------------------------------------------
* CMSIS-RTOS 'main' function template
*---------------------------------------------------------------------------*/
#include "RTE_Components.h"
#include CMSIS_device_header
#include "cmsis_os2.h"
#include "stm32f2xx_hal.h"
#include "stm32f2xx_hal_gpio.h"
#include "main.h"
//osMutexId_t mutex_id;
/*----------------------------------------------------------------------------
* Application main thread
*---------------------------------------------------------------------------*/
__NO_RETURN void thread1 (void *argument) {
(void)argument;
uint32_t ii=0;
osMutexId_t mutex_id1;
__HAL_RCC_GPIOF_CLK_ENABLE(); // enabling the peripheral clock
// gpio structure initialization
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Mode= GPIO_MODE_OUTPUT_PP ;
GPIO_InitStructure.Pin= GPIO_PIN_0;
GPIO_InitStructure.Pull= GPIO_PULLUP;
GPIO_InitStructure.Speed= GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOF, &GPIO_InitStructure);
mutex_id1 = osMutexNew (NULL);
while(1)
{
for(ii=0;ii<100;ii++)
{
osMutexAcquire (mutex_id1, 100);
HAL_GPIO_TogglePin(GPIOF, GPIO_PIN_0);
osDelay(100);
osMutexRelease (mutex_id1);
}
ii=0;
}
}
/*----------------------------------------------------------------------------
* Application main thread
*---------------------------------------------------------------------------*/
__NO_RETURN void thread2 (void *argument) {
(void)argument;
osMutexId_t mutex_id2;
uint32_t jj=0;
__HAL_RCC_GPIOF_CLK_ENABLE(); // enabling the peripheral clock
// gpio structure initialization
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Mode= GPIO_MODE_OUTPUT_PP ;
GPIO_InitStructure.Pin= GPIO_PIN_0;
GPIO_InitStructure.Pull= GPIO_PULLUP;
GPIO_InitStructure.Speed= GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOF, &GPIO_InitStructure);
mutex_id2 = osMutexNew (NULL);
while(1)
{
for(jj=0;jj<100;jj++)
{
osMutexAcquire (mutex_id2,100);
HAL_GPIO_TogglePin(GPIOF, GPIO_PIN_0);
osDelay(1000);
osMutexRelease (mutex_id2);
}
jj=0;
}
}
/*----------------------------------------------------------------------------
* Application main thread
*---------------------------------------------------------------------------*/
__NO_RETURN void thread3 (void *argument) {
(void)argument;
osMutexId_t mutex_id3;
uint32_t kk=0;
__HAL_RCC_GPIOF_CLK_ENABLE(); // enabling the peripheral clock
// gpio structure initialization
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Mode= GPIO_MODE_OUTPUT_PP ;
GPIO_InitStructure.Pin= GPIO_PIN_0;
GPIO_InitStructure.Pull= GPIO_PULLUP;
GPIO_InitStructure.Speed= GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOF, &GPIO_InitStructure);
mutex_id3 = osMutexNew (NULL);
while(1)
{
for(kk=0;kk<100;kk++)
{
osMutexAcquire (mutex_id3, 100);
HAL_GPIO_TogglePin(GPIOF, GPIO_PIN_0);
osDelay(500);
osMutexRelease (mutex_id3);
}
kk=0;
}
}
/*----------------------------------------------------------------------------
* Application main thread
*---------------------------------------------------------------------------*/
__NO_RETURN static void app_main (void *argument) {
(void)argument;
osThreadNew(thread1, NULL, NULL);
osThreadNew(thread2, NULL, NULL);
osThreadNew(thread3, NULL, NULL);
while(1);
}
int main (void) {
// System Initialization
SystemCoreClockUpdate();
// ...
osKernelInitialize(); // Initialize CMSIS-RTOS
osThreadNew(app_main, NULL, NULL); // Create application main thread
osKernelStart(); // Start thread execution
while(1);
}The output shows threads are not synchronized.
Here I am aware of linux threads(mutex) concepts.
same thing I am implemented in RTOS with little changes .
an any one help to solve this problem.
Thanks.