HPDMA does not seem to work with FMC memory-to-memory?
I've got an STM32H7RS, and am attempting to use HPDMA to do a memory-to-memory transfer where one side is the FMC.
The transfer works perfectly if I use GPDMA.
With the exact same code (just replacing the GPDMA handle with an HPDMA one) does not work (it returns an error from HAL_DMA_PollForTransfer) and reports:
State: HAL_DMA_STATE_READY
Error: HAL_DMA_ERROR_DTE
I've initialized HPDMA with the exact same parameters (and I've made sure to enable the HPDMA clock with __HAL_RCC_HPDMA1_CLK_ENABLE() at the top of MX_HPDMA1_Init()).
My MX_HPDMA1_Init():
/* USER CODE BEGIN HPDMA1_Init 0 */
__HAL_RCC_HPDMA1_CLK_ENABLE();
HAL_NVIC_SetPriority(HPDMA1_Channel12_IRQn, 8, 0);
HAL_NVIC_EnableIRQ(HPDMA1_Channel12_IRQn);
/* USER CODE END HPDMA1_Init 0 */
/* USER CODE BEGIN HPDMA1_Init 1 */
/* USER CODE END HPDMA1_Init 1 */
handle_HPDMA1_Channel12.Instance = HPDMA1_Channel12;
handle_HPDMA1_Channel12.Init.Request = DMA_REQUEST_SW;
handle_HPDMA1_Channel12.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
handle_HPDMA1_Channel12.Init.Direction = DMA_MEMORY_TO_MEMORY;
handle_HPDMA1_Channel12.Init.SrcInc = DMA_SINC_INCREMENTED;
handle_HPDMA1_Channel12.Init.DestInc = DMA_DINC_INCREMENTED;
handle_HPDMA1_Channel12.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_WORD;
handle_HPDMA1_Channel12.Init.DestDataWidth = DMA_DEST_DATAWIDTH_WORD;
handle_HPDMA1_Channel12.Init.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
handle_HPDMA1_Channel12.Init.SrcBurstLength = 8;
handle_HPDMA1_Channel12.Init.DestBurstLength = 8;
handle_HPDMA1_Channel12.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT1|DMA_DEST_ALLOCATED_PORT1;
handle_HPDMA1_Channel12.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_HPDMA1_Channel12.Init.Mode = DMA_NORMAL;
if (HAL_DMA_Init(&handle_HPDMA1_Channel12) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMA_ConfigChannelAttributes(&handle_HPDMA1_Channel12, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
My DMA code is:
uint8_t __attribute__((aligned(32))) local_dma_buf[8192 * 4];
#define DMA_HANDLE (&handle_GPDMA1_Channel12)
...
main()
{
...
uint32_t src_addr = (uint32_t)&FpgaMem.fifo;
uint32_t dst_addr = (uint32_t)&local_dma_buf[0];
if (HAL_DMA_Start(DMA_HANDLE, src_addr, dst_addr, 1024) != HAL_OK) {
ERROR("Could not start DMA");
} else {
if (HAL_DMA_PollForTransfer(DMA_HANDLE, HAL_DMA_FULL_TRANSFER, 1000) != HAL_OK) {
ERROR("Could not poll for transfer error dmaErr: 0x%lx dmaState: 0x%x",
HAL_DMA_GetError(DMA_HANDLE), HAL_DMA_GetState(DMA_HANDLE));
}
...
With DMA_HANDLE as shown, all works great. With DMA_HANDLE as &handle_HPDMA1_Channel12, it reports the state/error.
If it matters the FpgaMem is mapped at 0x60000000 in a MPU_TEX_LEVEL2 region (device).
Any suggestions would be greatly appreciated. Thanks!