Question
I am designing a board with STM32 device of P/N STM32G4A1KEUx. I am trying to see if I need to have an external pull up on the USB-FS D+ line for detection. The usual application note don't seem to include this device as it looks.
I am designing a board with STM32 device of P/N STM32G4A1KEUx. I am trying to see if I need to have an external pull up on the USB-FS D+ line for detection. The usual application note don't seem to include this device as it looks. Does this device has a pull up embedded for the USB detection If not can I still use the usual 1.5k on the D+ line?