I can't use function HAL_FLASH_Program to program same memory address twice
When I call function HAL_FLASH_Program twice with the same Flash address, the second call is ignored. See test code below.
int8_t buffer1[16] = {0x00,0x01,0x02,0x03,0x04,0x05,0x06,0x07,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF};
int8_t buffer2[16] = {0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0xFF,0x08,0x09,0x0A,0x0B,0x0C,0x0D,0x0E,0x0F};
EraseIntFlash( 0x08200000, 0x08300000 );
HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, 0X0820000, buffer1);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, 0X0820000, buffer2);
In Memory Browser, I expect:
0x08200000 03020100 07060504 0B0A0908 0F0E0D0C
But I get:
0x08200000 03020100 07060504 FFFFFFFF FFFFFFFF
What is going on? I really need this to work. Can anyone provide insight or solution or workaround?
Jim Eno