I found a bug in HAL_RCC_OscConfig for stm32f2xx (file stm32f2xx_hal_rcc.c).
When this function is called with the OSC configured, e.g. from bootloader, it checks if the PLLM/N/P/Q in RCC PLLCFGR reg are the same as requested. That check fails, even if the parameters in the second config request are the same.
Problem is located in following part of the code:
else
{
/* Do not return HAL_ERROR if request repeats the current configuration */
uint32_t pllcfgr = RCC->PLLCFGR;
if((READ_BIT(pllcfgr, RCC_PLLCFGR_PLLSRC) != RCC_OscInitStruct->PLL.PLLSource) ||
(READ_BIT(pllcfgr, RCC_PLLCFGR_PLLM) != RCC_OscInitStruct->PLL.PLLM) ||
((READ_BIT(pllcfgr, RCC_PLLCFGR_PLLN) >> RCC_PLLCFGR_PLLN_Pos) != RCC_OscInitStruct->PLL.PLLN) ||
(READ_BIT(pllcfgr, RCC_PLLCFGR_PLLP) != RCC_OscInitStruct->PLL.PLLP) ||
(READ_BIT(pllcfgr, RCC_PLLCFGR_PLLQ) != RCC_OscInitStruct->PLL.PLLQ))
{
return HAL_ERROR;
}
}PLLP and PLLQ needs shifting before checking, PLLP needs mapping, too.
The following code worked for me:
else
{
/* Do not return HAL_ERROR if request repeats the current configuration */
uint32_t pllcfgr = RCC->PLLCFGR;
if((READ_BIT(pllcfgr, RCC_PLLCFGR_PLLSRC) != RCC_OscInitStruct->PLL.PLLSource) ||
(READ_BIT(pllcfgr, RCC_PLLCFGR_PLLM) != RCC_OscInitStruct->PLL.PLLM) ||
((READ_BIT(pllcfgr, RCC_PLLCFGR_PLLN) >> RCC_PLLCFGR_PLLN_Pos) != RCC_OscInitStruct->PLL.PLLN) ||
((READ_BIT(pllcfgr, RCC_PLLCFGR_PLLP) >> RCC_PLLCFGR_PLLP_Pos) != (RCC_OscInitStruct->PLL.PLLP >> 1) - 1) ||
((READ_BIT(pllcfgr, RCC_PLLCFGR_PLLQ) >> RCC_PLLCFGR_PLLQ_Pos) != RCC_OscInitStruct->PLL.PLLQ))
{
return HAL_ERROR;
}
}Thought it would be worth reporting, as others might run into the same issue.
Regards,