Skip to main content
Graduate
August 21, 2023
Solved

I have 2 transceivers with stm32 and lora. I want to send signal from the transmitter and wake up th

  • August 21, 2023
  • 1 reply
  • 1504 views

Stm32 ve lora ile 2 alıcı-vericim var. Vericiden sinyalde oluşan ve alıcıyı uyandırmak istiyorum. Bunu nasıl araştırmalıyım?

Telsiz cihaz stm32 mikroişlemci ile çalışır.

bileşen lora(e220) ile aktarılır. Farklı bir modül de kullanıyorum.

derin uykuda olan cihaz rf sinyali ile çalışmak istiyorum.Cevaplarınız için teşekkür ederim.

    This topic has been closed for replies.
    Best answer by Tesla DeLorean

    Perhaps you can use CAD (Channel Activity Detection) to generate DIO / EXTI to wake?

    https://www.thethingsnetwork.org/forum/t/channel-activity-detection-cad-implementation-of-lora/13373

    1 reply

    Graduate II
    August 21, 2023

    "I have 2 transceivers with stm32 and lora. I want to wake up the receiver which is formed in the signal from the transmitter. How should I research this? The wireless device works with the stm32 microprocessor. the component is transferred with lora(e220). I am also using a different module. I want to work with device rf signal which is in deep sleep. Thank you for your answers."

    Yeah, not sure how you're going to pull it out of deep sleep. You'd perhaps need something synchronized with time and able to turn on when you expect the signals. Or partition the listening devices in your system so they can wake up the rest of the system when a message that is directed toward them is detected.

    YBAYR.1Author
    Graduate
    August 21, 2023

    I understand. Thank you very much for your reply. I am not sure if such a system is possible. Waking up a deep sleep device with an RF signal

    Graduate II
    August 21, 2023

    Perhaps you can use CAD (Channel Activity Detection) to generate DIO / EXTI to wake?

    https://www.thethingsnetwork.org/forum/t/channel-activity-detection-cad-implementation-of-lora/13373