I wish to add a new interface to the existing custom HID STM32 library
Hi,
I am developing an application with one configuration descriptor & 2 interfaces with 2 endpoints each. The endpoint (CUSTOM_HID) that comes as default while setting up the project via cubeIDE seems to be working alright. I can send and receive data correctly in this interface.
But when I add another interface with two of its new endpoints, the transmission (from device to host) using the in endpoint does not work & generates a pipe error on linux (libusb). Any idea why this could be occuring? Do I need to enable the macro indicating that I want to make the USB device a composite one?
Thanks