Skip to main content
Visitor II
May 20, 2020
Question

I would like to run X-CUBE-AZURE Cloud Connectivity Demonstration with P-L496G-CELL02. I entered network configuration setings for external SIM card. After that program doesn't continue , so I can't configure connection to Azure IoT hub.

  • May 20, 2020
  • 3 replies
  • 1026 views

 Starting Main Thread...

*************************************************************

***  STM32 IoT Discovery kit for

***   STM32F413/STM32F769/STM32L475/STM32L496 MCU

***  X-CUBE-AZURE Cloud Connectivity Demonstration

***  FW version: 1.2.1 - 07-November-2019 03:05:43 PM

*************************************************************

*** Board personalization ***

- Network Interface initialized:

Push the User button (Blue) within the next 5 seconds if you want to update the Cellular network configuration.

Your Cellular parameters need to be entered to proceed.

Select the SIM slot (0 - External, 1 - Internal):0

You have selected the external SIM.

Enter Sim Operator Access Point Code (e.g. EM or ESEYE1 etc): izimobil

You have entered <izimobil> as the Sim Operator Access Point Code.

Enter the username (it can be NULL) (max 16 char): izimobil

You have entered <izimobil> as the username.

Enter the password (it can be NULL) (max 16 char): izimobil

You have entered <izimobil> as the password.

- Network Interface starting:

*** C2C connection ***

Initializing the cellular module

- Network Interface connecting:

Trying to connect with the external SIM

Waiting for BG96 modem running

Signal not known or not detectable yet (be patient)

............................................................

...........

Signal Level: -75 dBm

...........

C2C module registered

Registration done in 80026 msseconds

Retrieving the cellular operator: "izimobil izimobil"

Module initialized successfully: Quectel

ProductID: BG96

FW version: BG96MAR02A06M1G

SIM Id (IccID): 8938641142000150266F

- Network Interface started:

  - Device Name : Quectel.

  - Device ID : BG96.

  - Device Version : BG96MAR02A06M1G.

Waiting for BG96 modem running

Waiting for BG96 modem running

    This topic has been closed for replies.

    3 replies

    ST Employee
    May 20, 2020

    Hello,

    BG96MAR02A06M1G is the factory FW cellular modem and must be upgraded.

    I would suggest to upgrade the BG96 FW modem version with a newest version.

    For instance, you can find BG96MAR02A07M1G_010 under https://stm32-c2c.com in precompiled Demos Repository.

    Thierry

    ST Employee
    May 20, 2020

    did you try to use the network operator provided with the board ? ("EM" = Emnify)

    did it work ?

    MZotl.1Author
    Visitor II
    May 22, 2020

    I tried upgrading FW and it works with any SIM card now. Thank you very much.