I2C HAL_BUSY Debugging Help
Currently I am trying to interface with a LM75A temperature sensor using the STM32F446RE nucleo board.
From the datasheet of the LM75A, I gathered that the sensor, returns a temperature measurement without any configuration.
So I tried to simply hook up the LM75A (with floating Address Pins) and connecting it to the I2C1 port on the STM32.
Addressing the slave on the given default address of 0x48h
The code below returns HAL_BUSY, and locks up. Since I do not have a Logic Analyzer at home, I cannot manually debug what is going on.
#include "COM_Driver.h"
#include "LM75A_Driver.h"
#include <string.h>
int main(){
LM75_Init();
COM_Init();
uint8_t data[2];
float temperature;
char tes[8];
while (1)
{
HAL_StatusTypeDef status = LM75_ReadReg(LM75A_ADDRESS, LM75_TEMP_REG, data, 2);
if (status != HAL_OK)
{
// Handle I2C communication error
continue; // Skip to the next iteration of the loop
}
temperature = (float)((data[0] << 8) | data[1]) / 256;
sprintf(tes, "%f\n", temperature);
COM_printf(tes);
COM_printf("Hi!");
HAL_Delay(1000);
}
}LM75 Driver is simply an abstraction of HAL_MASTER_TRANSMIT()
#include "LM75A_Driver.h"
I2C_HandleTypeDef hi2c;
// Initialize I2C peripheral and GPIO pins
void LM75_Init(void)
{
// Enable clock for I2C peripheral and GPIO port
I2Cx_CLK_ENABLE();
I2Cx_GPIO_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct = {0};
// Configure SCL, SDA pins as alternate function
GPIO_InitStruct.Pin = I2Cx_SCL_PIN | I2Cx_SDA_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = I2Cx_AF;
__HAL_RCC_GPIOB_CLK_ENABLE();
HAL_GPIO_Init(I2Cx_GPIO_PORT, &GPIO_InitStruct);
__HAL_RCC_I2C1_CLK_ENABLE();
// I2C peripheral configuration
hi2c.Instance = I2Cx;
hi2c.Init.ClockSpeed = 300000; // Adjust as needed
hi2c.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c.Init.OwnAddress1 = 0;
hi2c.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c.Init.OwnAddress2 = 0;
hi2c.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c) != HAL_OK)
{
// Initialization Error
Error_Handler();
}
}
// Write data to an I2C device
HAL_StatusTypeDef LM75_WriteReg(uint8_t device_address, uint8_t register_address, uint8_t *data, uint16_t size)
{
if (register_address == LM75_TEMP_REG || register_address == LM75_INFO_REG)
{
return HAL_ERROR;
}
return HAL_I2C_Master_Transmit(&hi2c, device_address, data, size, HAL_MAX_DELAY);
}
// Read data from an I2C device
HAL_StatusTypeDef LM75_ReadReg(uint8_t device_address, uint8_t register_address, uint8_t *data, uint16_t size)
{
return HAL_I2C_Master_Receive(&hi2c, device_address, data, size, HAL_MAX_DELAY);
}And COM_printf() is a implemented function to print the temperature data to my computers terminal! There are no bugs in that piece of code.
Also I have not handled the HAL Errors since this is a prototype code.
If you have any suggestions from my code code that would be much appreciated.