I2C HAL_I2C_SlaveRxCpltCallback is not called on slave after master transmit
Hi,
I am trying to establish I2C communication between STM32C011 (Master) and STM32C031 Nucleo Board (Slave).
I transmit a message from the master, however, the slave side sees that the master wants to write to the slave (using HAL_I2C_AddrCallback) however, the HAL_I2C_SlaveRxCpltCallback is never called.
In another post, I see that the buffer length may be an issue, so I tried to transmit just one character but to no avail.
ChatGPT suggested I shouldn't re-arm the HAL_I2C_Slave_Receive_IT function as it can cause it to get stuck. I tried it with and without but same result.
I see "Master wants to write to slave" only once upon power up/reset of the slave MCU.
Master Side:
#include "main.h"
#define SLAVE_ADDR 0x42 << 1
I2C_HandleTypeDef hi2c1;
SPI_HandleTypeDef hspi1;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
static void MX_I2C1_Init(void);
uint8_t TX_Buffer [] = "A";
//uint8_t TX_Buffer [] = "MasterToSlave"; // DATA to send
uint8_t RX_Buffer [14];
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_SPI1_Init();
MX_I2C1_Init();
toggleRED(4,4,100);
while (1)
{
master_send_receive();
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
__HAL_FLASH_SET_LATENCY(FLASH_LATENCY_1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_I2C1_Init(void)
{
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x10805D88;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
{
Error_Handler();
}
}
static void MX_SPI1_Init(void)
{
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_16BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
HAL_GPIO_WritePin(GPIOC, Bank2RED_Pin|Bank1RED_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, Bank1Latch_Pin|Bank2Latch_Pin|Bank3Latch_Pin|Bank4Latch_Pin
|Bank34WHT_Pin, GPIO_PIN_RESET);
GPIO_InitStruct.Pin = Bank2RED_Pin|Bank1RED_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = Bank1Latch_Pin|Bank2Latch_Pin|Bank3Latch_Pin|Bank4Latch_Pin
|Bank34WHT_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = Bank4BTN_Pin|Bank3BTN_Pin|Bank1BTN_Pin|Bank2BTN_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);
}
void master_send_receive(void)
{
HAL_Delay(1000);
//if (HAL_I2C_IsDeviceReady (&hi2c1, SLAVE_ADDR, 3, 1000) == HAL_OK)
{
toggleRED(1,4,100);
if (HAL_I2C_Master_Transmit(&hi2c1, SLAVE_ADDR, TX_Buffer, strlen((char*)TX_Buffer), 1000) == HAL_OK)
{
toggleRED(3,1,1000);
}
if (HAL_I2C_Master_Receive(&hi2c1, SLAVE_ADDR, RX_Buffer, sizeof(RX_Buffer), 1000) == HAL_OK)
{
toggleRED(4,2,100);
if ((RX_Buffer[0] != 0)||(RX_Buffer[1] != 0)||(RX_Buffer[2] != 0)||(RX_Buffer[3] != 0)||(RX_Buffer[4] != 0)||(RX_Buffer[5] != 0)||(RX_Buffer[6] != 0))
{
HAL_GPIO_TogglePin(RED_GPIO_PORT[1], RED_GPIO_PIN[1]);
}
}
}
}
void toggleRED(uint8_t bank, uint8_t blinks, uint16_t msDelay)
{
for(uint8_t i=0; i<blinks; i++)
{
HAL_GPIO_TogglePin(RED_GPIO_PORT[bank], RED_GPIO_PIN[bank]);
HAL_Delay(msDelay);
HAL_GPIO_TogglePin(RED_GPIO_PORT[bank], RED_GPIO_PIN[bank]);
HAL_Delay(msDelay/2);
}
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
}
#endif
Slave Side:
#include "main.h"
#include <stdio.h>
I2C_HandleTypeDef hi2c1;
TIM_HandleTypeDef htim3;
UART_HandleTypeDef huart2;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_TIM3_Init(void);
static void MX_USART2_UART_Init(void);
uint8_t Slave_TX_Buffer [] = "SlaveToMaster";
uint8_t Slave_RX_Buffer [1];
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
MX_TIM3_Init();
MX_USART2_UART_Init();
HAL_TIM_Base_Start_IT(&htim3);
__enable_irq();
toggleLED(4,100);
if (HAL_I2C_EnableListen_IT(&hi2c1) != HAL_OK)
{
printf("Failed to enable I2C listen mode\r\n");
}
while (1)
{
//HAL_Delay(1000);
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
__HAL_FLASH_SET_LATENCY(FLASH_LATENCY_1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_I2C1_Init(void)
{
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x10805D88;
hi2c1.Init.OwnAddress1 = 132;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
{
Error_Handler();
}
}
static void MX_TIM3_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
htim3.Instance = TIM3;
htim3.Init.Prescaler = 47999;
htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
htim3.Init.Period = 9999;
htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}
static void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 57600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
HAL_GPIO_WritePin(GRNLED_GPIO_Port, GRNLED_Pin, GPIO_PIN_RESET);
GPIO_InitStruct.Pin = BLUBTN_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(BLUBTN_GPIO_Port, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GRNLED_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GRNLED_GPIO_Port, &GPIO_InitStruct);
HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);
}
int __io_putchar(int ch)
{
HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
return ch;
}
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
HAL_GPIO_TogglePin(GRNLED_GPIO_Port, GRNLED_Pin);
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
printf("10 Seconds Elapsed\r\n");
}
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
if (hi2c->Instance == I2C1)
{
if (TransferDirection == I2C_DIRECTION_TRANSMIT)
{
printf("Master wants to write to slave\r\n");
HAL_I2C_Slave_Receive_IT(hi2c, Slave_RX_Buffer, sizeof(Slave_RX_Buffer));
}
else if (TransferDirection == I2C_DIRECTION_RECEIVE)
{
printf("Master wants to read from slave\r\n");
HAL_I2C_Slave_Transmit_IT(hi2c, Slave_TX_Buffer, sizeof(Slave_TX_Buffer));
}
}
}
void HAL_I2C_ListenCpltCallback(I2C_HandleTypeDef *hi2c)
{
if (hi2c->Instance == I2C1)
{
printf("Listen complete. Re-enabling listen mode.\r\n");
HAL_I2C_EnableListen_IT(hi2c);
}
}
void HAL_I2C_SlaveRxCpltCallback(I2C_HandleTypeDef *hi2c)
{
{
printf("SlaveRxCpltCallback triggered. Data: %s\r\n", Slave_RX_Buffer);
toggleLED(1,1000);
HAL_I2C_Slave_Receive_IT(&hi2c1, Slave_RX_Buffer, sizeof(Slave_RX_Buffer));
}
}
void HAL_I2C_SlaveTxCpltCallback(I2C_HandleTypeDef *hi2c)
{
if (hi2c->Instance == I2C1)
{
printf("SlaveRxCpltCallback triggered. Data: %s\r\n", Slave_RX_Buffer);
HAL_GPIO_WritePin(GRNLED_GPIO_Port, GRNLED_Pin, GPIO_PIN_SET);
printf("I2C message sent from tx callback interrupt.\r\n");
HAL_I2C_Slave_Transmit_IT(&hi2c1, Slave_TX_Buffer, sizeof(Slave_TX_Buffer));
}
}
void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *hi2c)
{
if (hi2c->Instance == I2C1)
{
printf("I2C error occurred. Re-arming receive.\r\n");
HAL_I2C_Slave_Receive_IT(&hi2c1, Slave_RX_Buffer, sizeof(Slave_RX_Buffer));
}
}
void toggleLED(uint8_t blinks, uint16_t msDelay)
{
for(uint8_t i=0; i<blinks; i++)
{
HAL_GPIO_TogglePin(GRNLED_GPIO_Port, GRNLED_Pin);
HAL_Delay(msDelay);
HAL_GPIO_TogglePin(GRNLED_GPIO_Port, GRNLED_Pin);
HAL_Delay(msDelay/2);
}
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line)
{
}
#endif