Question
I2S/SPI interrupt fires only once, when restarted in IRQ routine (STM32H503)
I have set up an I2S interface. The idea is to send it an initial HAL_I2S_Transmit_IT() request.
In the ISR of SPI2 I'm sending the next HAL_I2S_Transmit_IT() and this way the transmit should be continously kept running.
What happens is, that the SPI ISR is entered once. The HAL_I2S_Transmit_IT() issued within the ISR, doesn't fire the subsequent IR. Why?