Skip to main content
Visitor II
June 28, 2022
Question

im trying to write data on sd card but it Doesn't Work :

  • June 28, 2022
  • 1 reply
  • 885 views

 I use a simple code in stm32 for SD card.

The code is written in "int main(void)" section. I am trying to configure a SD card so that as soon as the STM32F750vbt6 turn on, a file is created in the SD card and a text is written in the file.

when I turn the STM32F750vbt6 on, this does not happen and nothing is written in the SD card but when the code reaches to the "while" section (I have written an LED blink code inside the while section) and I reset the micro controller using RST pin of the STM32F750vbt6, the device works properly and a text is written in the sd card.

How can I fix this? Why is there a need for resetting the device for the code to work?

const char wtext[] = "hi world";
 int main(void)
 {
 FRESULT res; /* FatFs function common result code */
 uint32_t byteswritten, bytesread; /* File write/read counts */
 MPU_Config();
 HAL_Init();
 SystemClock_Config();
 MX_GPIO_Init();
 MX_SDMMC1_SD_Init();
 MX_FATFS_Init();
 if(retSD == 0)
 {
 if(f_mount(&SDFatFs, (TCHAR const*)SDPath, 0) == FR_OK)
 {
 if(f_open(&MyFile, "file.txt", FA_CREATE_ALWAYS | FA_WRITE) ==FR_OK)
 {
 f_write(&MyFile, wtext, sizeof(wtext), (void*)&byteswritten);
 f_close(&MyFile);
 }
 }
 }
 FATFS_UnLinkDriver(SDPath);
 while (1)
 {
 HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);
 HAL_Delay(2000);
 HAL_GPIO_WritePin(LED1_GPIO_Port, LED2_Pin, GPIO_PIN_RESET);
 HAL_Delay(2000);
 }
 }

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 6, 2022

    Hi @YKh.1​ ,

    If you use the STM32CubeIDE, I advise you to follow this article may help you.

    Kaouthar