Implementing FRS on G474
Dear ST Community
I recently purchased two sets of Nucleo-DRP1M1+NucleoG474, and now I want to implement FRS functionality on these two boards. Currently, I have set one of the default power roles to Source, enabled FRS_TX, and the other to Sink. After connecting the two devices together, FRS switching cannot be triggered, and when I was debugging on the Sink side, I found that the FRS interrupt in the code on the Sink side is in a blocked state, and I don't know how to turn it on.

Best regards.

I added the FRS macro definition, but there is a function error inside that I cannot find