Question
In our project, we are using STM32G431KB microcontroller and TCPP01-M12 for type C protection
1) CC1 and CC2 connections from microcontroller are properly connected to TCPP01-M12.
2) When TCPP01-M12 is separately powered up, input given to CC1 and CC2 appears on CC1_C & CC2_C
3) When input to CC1 and CC2 are given from the controller, the voltage is getting dropped in the input side of TCPP01-M12
I have attached the screenshots of the schematics for reference