incorporate LwIP_UDP_Echo_Server example code into another project
Want to incorporate LwIP_UDP_Echo_Server example code for NUCELO-H723ZG with another project which has ADC, DMA, and timer system setup for sampling data. Issue is there is no .ioc file for the example code and when trying to look into the code manually for the parameters to feed into cubeMX when trying to configure a new project, there was some values that were missing, and some that were showing up as invalid (even though when testing the example code it was working fine). A bit lost and have been spending a lot of time trying to identify how to go about this. Any help on this would be appreciated.