Input Capture - Trouble Measuring Frequency
Hello, i have been trying to measure the frequency of a pwm signal using input capture. I am using Nucleo-F429ZI I want to print the values of the frequency of the signal in question with UART. The frequency of my signal is 100 kHz but I read stuff like these on my serial monitor: (I printed diff instead of frequency to see what is the issue, it is the same with frequency just with bigger values.)
The oldest data was removed. Continue...
6
371
305
108
628
174
10578
482
410
364
375
355
365
365
365
13157
516
385
285
50218
20130
20048
20005
19942
20044
20016
19963
(I cut most of the data so that the post isn't too long but it is roughly like this. Constant values near 365 and occasianl continous irrelevant high values)
Below is the relevant parts of my code:
...
/* USER CODE BEGIN 0 */
uint32_t captureValue = 0;
uint32_t previousCaptureValue = 0;
uint16_t diff;
uint16_t frequency = 0;
char uart_buffer[32];
static uint8_t first_capture_flag = 1;
/* USER CODE END 0 */
...
int main(void){
...
HAL_TIM_IC_Start_IT(&htim3, TIM_CHANNEL_1);
...
}
...
/* USER CODE BEGIN 4 */
//CK_CNT = TIM_CLK / (PSC + 1) = PCLK1 * 2 / (PSC + 1) = 90 / (90 - 1 +1 ) = 1 MHz => counter_period = 1/1 MHz = 1 us
//
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
captureValue = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);
if(first_capture_flag){
previousCaptureValue = captureValue;
first_capture_flag = 0;
}
if(captureValue > previousCaptureValue){
diff = captureValue - previousCaptureValue;
frequency = 1000000 / diff;
}
else if(captureValue < previousCaptureValue){
diff = 65535 - previousCaptureValue + captureValue;
frequency = 1000000 / diff;
}
previousCaptureValue = captureValue;
if (frequency > 90000 && frequency < 110000){ //freq = 100 kHz
// sprintf(uart_buffer, "%hu\n", frequency);
// HAL_UART_Transmit(&huart4, (uint8_t*)uart_buffer, strlen(uart_buffer), 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14, GPIO_PIN_SET);
}
else if (frequency > 45000 && frequency < 55000){ //freq = 50 kHz
// sprintf(uart_buffer, "%hu\n", frequency);
// HAL_UART_Transmit(&huart4, (uint8_t*)uart_buffer, strlen(uart_buffer), 100);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14, GPIO_PIN_RESET);
}
sprintf(uart_buffer, "%hu\n", diff);
HAL_UART_Transmit(&huart4, (uint8_t*)uart_buffer, strlen(uart_buffer), 100);
}
/* USER CODE END 4 */
...