Integration of a position dependent library (binary) in a threadx module ( position independent )
Hi, I am working on threadx.
So to set the context,
Module manager will host modules.
All the modules are compiled as position independent. Module manager however is not position independent.
Scenario : a third party library (binary) has to be used in a module.
Problem : the library binary is not compiled as position independent.
------------------------------------------------------------------------------------------------------------------------------
- Any suggestions to link the binary with the module?
------------------------------------------------------------------------------------------------------------------------------
- I have been theorizing to compile the library with the module manager and implement a function pointer interface. Any remarks/suggestions for the same are welcome.
Thank you!