Internal temperature Sensor STM32H743ZIT6
I am using internal Temperature Sensor stm32h743zit6 , i notice that when i connect power some time after that it stable temperature approximately 46 degree or 47 degree, after i start streaming it came temperature also stable on this 46 degree or 47 degree temperature ,so when i work or not work continues but i give continues power always stable it give stable temperature after some time 46 degree or 47 ..but when i heat external 50 degree Celsius then it came internal Temperature 51 degree Celsius , again i heat external 60 degree Celsius then it came internal Temperature 58 degree Celsius so can you tell me behavior of internal Temperature Sensor stm32h743zit6!!!!!!!!
so it is true that if i work or not but it give continues power supply than after some time it will always stable 46 or 47 degree Celsius and if i do external heat it will increase according to external heat provide if it true than explain it if false than why it came ????????????????????????
but i doing some internal work just like streaming than it is possible to increase temperature from the stable temperature ,it is possible to increase or it give stable temperature 46 0r 47 degree ?????????????