Interrupt driven I2C traffic not working before FreeRTOS is up and running.
We have a project on an STM32H750 using FreeRTOS and I am trying to access an I2C device after the peripheral inits but before the FreeRTOS init and scheduler start in Main.c but I get no interrupts from the I2C port. I have checked that the interrupts are enabled for the port. If I do the exact same thing in a RTOS task later it works fine. If I do I2C traffic without interrupts that works fine too so the port is working. Anyone knows why?