Skip to main content
Visitor II
November 26, 2021
Solved

Is current-limited power switch needed inOTG_HS "peripheral only" design ?

  • November 26, 2021
  • 1 reply
  • 754 views

It 's seem to me there is an error page 2651 of RM0468, STMH730 reference manual.

the figure 782 has a Current limited power switch in the design, but if un understand corretly, is only need in OTG host or dual role device.

Am I correct ? there is no need of current limited power switch on Vbus in peripheral only ?

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome, @Tbill.1​, to the community!

    Yes, you are right. It is also mentioned in the caption:

    1. (Instead) Use a regulator to build a bus-powered device.

    Regards

    /Peter

    1 reply

    Technical Moderator
    November 26, 2021

    Welcome, @Tbill.1​, to the community!

    Yes, you are right. It is also mentioned in the caption:

    1. (Instead) Use a regulator to build a bus-powered device.

    Regards

    /Peter