Is HAL_UART_Transmit atomic per byte?
(STM32F103C8)
My program continuously sends UART messages with regular blocking calls like this:
HAL_UART_Transmit(&huart1, buf, size, timeout);
The result on my logic analyzer normally looks like:

I also handle interrupts coming from HAL_SPI_TxRxCpltCallback at 1kHz. When this coincides with a UART transmission, the result looks like this:


The SPI interrupt causes a slight delay in UART transmission, but it never seems to corrupt the transmitted data by getting "in between" the bits of each byte and messing up the timing. I ran a test for many hours and everything was fine.
Is this behavior something I can depend on to always be true? If so, I would imagine that to accomplish this the UART is disabling interrupts during the time it is transferring each byte? I have a bunch of other timer interrupt driven code that is quite time-sensitive, just trying to understand if the UART will affect that.