Skip to main content
Visitor II
July 10, 2020
Question

Is it required to have HSE clock source for custom bootloader using CAN bus for STM32F446RE

  • July 10, 2020
  • 1 reply
  • 762 views

Hello,

In the application note AN2606, it is mentioned that ST's bootloader for STM32F446RE requires HSE clock if CAN bus is used to upload the hex file.

Now, if I am writing my own custom bootloader to upload the code via CAN, would I still need the HSE clock. Is possible to route HSI clock for the system clock and APB1

Thank you.

Snippet from AN2606

0693W000001sg84QAA.png

    This topic has been closed for replies.

    1 reply

    Graduate II
    July 10, 2020

    You can choose to clock it via any source you want, even ones which are out-of-spec. As long as you're willing to deal with things not work on an occasional unit, and support of that, you can use the HSI