Is the ROM bootloader source available somewhere?
I'm planning to use the built-in ROM bootloader in an STM32F4 chip for DFU uploads and having a hard time figuring out how it works exactly (in particular what pins it initializes at what moment in the boot process, and what I need to do externally to prevent it from going into e.g. SPI or UART mode). The documentation is missing some details (and experiments also give me puzzling results), so I'm looking for some more specific insight in the workings of this bootloader, which would be perfectly solved by looking at the source code.
I've read some earlier related posts, and I suspect that the sources are not currently available, but maybe someone at ST will see this as a request to change that? I would think there will not be any secrets in their bootloader sources, but it would make the bootloaders (and thus their hardware platform) a lot more usable.
Note that I realize that the ROM bootloader is not perfect and might not be a good basis for a custom bootloader, but that is not my goal (my goal is to understand and use the ROM bootloader). I also realize that the bootloader is in ROM and cannot be modified.
I also realize that using a custom bootloader in flash is also a commonly used option, but I'd prefer to use the builtin one (since that can certainly not be erased, and simplifies production).
I noticed @Community member mentioning in this topic that you can read back the compiled bootloader from ROM and disassemble that, which would also be helpful (but a lot harder to read, of course). He mentions his "own annotated listings", but without a link it seems. I wonder if there is any repository of such listings or dumps? If not, anyone aware of some tutorial on how to generate them? Though I guess it's a matter of dumping memory through SWD and then disassembling with something like `objdump`?