Skip to main content
Visitor II
August 28, 2023
Question

Issue in building SBSFU_Boot example for NUCLEO-WBA52CG

  • August 28, 2023
  • 0 replies
  • 788 views

Hi,

I'm facing an issue in building a SBSFU_Boot example for NUCLEO-WBA52CG.

The issue seems to be with the linkage error, for the Third_party files (mcuboot).

 

Please find the error message below:

 

C:/Users/zapk/STM32CubeIDE/workspace_1.13.1/SBSFU_Boot/STM32CubeIDE/Release

../postbuild.sh: cd: line 16: can't cd to C:/Users/zapk/STM32CubeIDE/workspace_1.13.1/SBSFU_Boot/STM32CubeIDE/../../Middlewares/Third_Party/mcuboot: No such file or directory

Windows_NT

Postbuild with python script

python: can't open file 'C:\\Users\\zapk\\STM32CubeIDE\\workspace_1.13.1\\SBSFU_Boot\\STM32CubeIDE\\Release\\scripts\\imgtool\\main.py': [Errno 2] No such file or directory

postbuild.sh failed

make[1]: *** [makefile:95: post-build] Error 1

make: *** [makefile:61: all] Error 2

"make -j16 all" terminated with exit code 2. Build might be incomplete.

 

13:56:25 Build Failed. 2 errors, 0 warnings. (took 8s.142ms)

    This topic has been closed for replies.