Skip to main content
Graduate II
January 22, 2025
Solved

Issue in Read and Write using SD_Card.

  • January 22, 2025
  • 1 reply
  • 430 views
The issue is that I am able to create a bin file, write data into the SD-Card properly. But when I read data, it is not proper, and the data is corrupted. It worked well previously but the same code is not working now. Could you please check where I am wrong. I am using STM32L496ZGT6. I am using a Micro SD Card adapter.

WRITING FUNCTION
 
void push_to_stack(data *newData) {
      fres = f_mount(&fs, "", 0);
if (fres == FR_OK) {
transmit_uart("Micro SD card is mounted successfully for writing!\n");
} else if (fres != FR_OK) {
transmit_uart("Micro SD card's mount error!\n");
}
 
      fres = f_open(&fil, "log-file.bin",  FA_WRITE| FA_OPEN_ALWAYS  );
if (fres != FR_OK) {
transmit_uart("Failed to open file for writing.\n");
f_mount(NULL, "", 1);  // Unmount before returning
}
fres = f_lseek(&fil, f_size(&fil));
    if (fres != FR_OK) {
        transmit_uart("Error seeking to the end of the file.\n");
        f_close(&fil);  // Close the file if seek fails
        f_mount(NULL, "", 1);  // Unmount before returning
        return;
    }
 
    // Write the structure to the file
    fres = f_write(&fil, newData, sizeof(data), &bytesWritten);
    if (fres == FR_OK && bytesWritten == sizeof(data)) {
        transmit_uart("Data successfully written to stack.\n");
    } else {
        transmit_uart("Error writing data to stack.\n");
    }
 
    fres = f_close(&fil);
    if (fres == FR_OK) {
    transmit_uart("The file is closed.\n");
    } else if (fres != FR_OK) {
    transmit_uart("The file was not closed.\n");
    }
 
    f_mount(NULL, "",1);
 
}
 
 
 
READ FUNCTION
void read_from_stack_and_send(uint32_t index) {
 
    // Mount the file system
    fres = f_mount(&fs, "", 0);
    if (fres != FR_OK) {
        transmit_uart("Failed to mount SD card.\n");
        return;
    } else {
        transmit_uart("SD card mounted successfully for reading.\n");
    }
 
    // Open file in read mode
    fres = f_open(&fil, "log-file.bin", FA_READ);
    if (fres != FR_OK) {
        transmit_uart("Failed to open file for reading.\n");
        return;
    } else {
        transmit_uart("File opened for reading successfully.\n");
    }
    fres = f_lseek(&fil,index * sizeof(data));
    if(fres != FR_OK){
    transmit_uart("Error reading data from file.\n");
    f_close(&fil);  // Close the file if seek fails
    f_mount(NULL, "", 1);  // Unmount before returning
    }
    // Read data sequentially
    data readData;
    UINT bytesRead;
 
   // while (1) {
        // Read a single `data` structure from the file
    memset(&readData, 0, sizeof(data));
        fres = f_read(&fil, &readData, sizeof(data), &bytesRead);
 
        if (fres != FR_OK) {
            transmit_uart("Error reading data from file.\n");
 
        }
 
        // Check if end of file reached
        if (bytesRead == 0) {
            transmit_uart("End of file reached.\n");
 
        }
 
        // Print the read data
        char msg[100];
        sprintf(msg, "ID: %d, Value: %d, Name: %s\n", readData.ID, readData.value, readData.ename);
        transmit_uart(msg);
  //  }
 
    // Close the file
    fres = f_close(&fil);
    if (fres != FR_OK) {
        transmit_uart("Failed to close the file.\n");
    } else {
        transmit_uart("File closed successfully.\n");
    }
 
    // Unmount the file system
    fres = f_mount(NULL, "", 1);
    if (fres != FR_OK) {
        transmit_uart("Failed to unmount SD card.\n");
    } else {
        transmit_uart("SD card unmounted successfully.\n");
    }
}
 
 
 
 
 
MAIN FUNCTION
    memset(buffer,0,sizeof(buffer));
    HAL_UART_Receive(&huart3, (uint8_t *)buffer, 100, 100);
    buffer[100]='\0';
    if(sscanf((char *)buffer,"UPDATE:%d,%d,%s",&cmdType,&value,name)==3){
    data received = {cmdType,value};
    strncpy(received.ename,name,sizeof(received.ename)-1);
    received.ename[sizeof(received.ename)-1]='\0';
    push_to_stack(&received);
    }
    else if(sscanf((char *)buffer,"INDEX:%d",&Index)==1){
    uint8_t buf[sizeof(data)];
    read_from_stack_and_send(Index);
    }

 

    This topic has been closed for replies.
    Best answer by vbk22398

    Issue resolved. Some changes I have added in the previous version and it is resolved today.

    1 reply

    vbk22398AuthorAnswer
    Graduate II
    January 22, 2025

    Issue resolved. Some changes I have added in the previous version and it is resolved today.