Issue to compile C and C++ with FreeRTOS, functions not recognized on stm32h7xx_it.c
Hi,
In order to compile FreeRTOS in C++, I did a makefile that compile FreeRTOS in C (to avoid void* issue not recognized by C++), and the other files with C++ including stm32h7xx_it.c on cpu Cortex-M7.
Whatever the options of compilation I am using (shared library of mixed compilation between C and C++), I have the same issue on some files like stm32h7xx_it.c.
It does not recognize the functions embedded inside the C file.
Examples of issues are described here:
Creating FreeRTOS lib ....
Linking output ELF file to OBJECTS ....
***/tools/windows/9-2020-q2-update/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: out_cm7/obj/Applications/CM7/src/stm32h7xx_it.o: in function `prvGetRegistersFromStack(unsigned long*)':
stm32h7xx_it.c:(.text+0x64): undefined reference to `prvGetRegistersFromStack'
***/tools/windows/9-2020-q2-update/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: libFreeRTOS.a: undefined reference to `ulApplicationGetNextSequenceNumber'
***/tools/windows/9-2020-q2-update/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: libFreeRTOS.a: undefined reference to `vApplicationGetIdleTaskMemory'
collect2.exe: error: ld returned 1 exit status
make[1]: *** [out_cm7/CM7.elf] Error 1
***/MakefileCM7.mk:288: recipe for target 'out_cm7/CM7.elf' failed
make[1]: Leaving directory '***'
make: *** [includeMakefileCM7] Error 2
makefile:65: recipe for target 'includeMakefileCM7' failed
"make -j all_CM7" terminated with exit code 2. Build might be incomplete.
If you alreadey raised this kind of issue, it would help otherwise we will stay in whole C.
Thank you for your help!
Kind regards,
Isabelle