Issues while initializing USB as Communication device class CDC using STM32Cube.
Hello everyone,
I am trying to use USB on the STM32 NUCLEO-L4RZI-P dev board to work as a Communication device class (CDC).
I have initialized the USB using the Cube IDE.
After initializing, I tried sending data using the " CDC_Transmit_FS( buffer, sizeof(buffer) ); "
This function is being called from the while(1) loop.
But I am facing some issue while doing so. When I tried tracing the issue, I found out that the while initializing, in function "USB_SetCurrentMode()" the HAL_Delay() never returns.
I am following these resources:
https://www.youtube.com/watch?v=h9T0RTu9Muc&list=PLnMKNibPkDnFFRBVD206EfnnHhQZI4Hxa&index=11
https://shawnhymel.com/1795/getting-started-with-stm32-nucleo-usb-virtual-com-port/