Jump from my own bootloader into my application NUCLEO-F429ZI
Hi,
I'm trying to write my own bootloader. It's located in 0x8000000 address of internal flash. I simply want to jump into 0x8080000 internal flash address when I press the external pushbutton connected to the EXTI. The code located into 0x8080000 just toggles a user led. I wrote my own bootloader code:
Bootloader
#define APPLICATION_BASE_ADDR 0x8080000
typedef void (*pFunction)(void); /* Function pointer definition */
/* ------------------------- Functions -------------------------------------- */
void Bootloader_JumpToApplication(void){
uint32_t JumpAddress = *(__IO uint32_t*)(APPLICATION_BASE_ADDR+4);
pFunction Jump = (pFunction)JumpAddress;
HAL_UART_DeInit(&huart3);
HAL_GPIO_DeInit(USER_Btn_GPIO_Port, USER_Btn_Pin);
HAL_GPIO_DeInit(GPIOC, RMII_MDC_Pin|RMII_RXD0_Pin|RMII_RXD1_Pin);
HAL_GPIO_DeInit(GPIOA, RMII_REF_CLK_Pin|RMII_MDIO_Pin|RMII_CRS_DV_Pin);
HAL_GPIO_DeInit(GPIOB, LD1_Pin|LD3_Pin|LD2_Pin);
HAL_GPIO_DeInit(RMII_TXD1_GPIO_Port, RMII_TXD1_Pin);
HAL_GPIO_DeInit(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin);
HAL_GPIO_DeInit(USB_OverCurrent_GPIO_Port, USB_OverCurrent_Pin);
HAL_GPIO_DeInit(GPIOA, USB_SOF_Pin|USB_ID_Pin|USB_DM_Pin|USB_DP_Pin);
HAL_GPIO_DeInit(USB_VBUS_GPIO_Port, USB_VBUS_Pin);
HAL_GPIO_DeInit(GPIOG, RMII_TX_EN_Pin|RMII_TXD0_Pin);
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOD_CLK_DISABLE();
__HAL_RCC_GPIOG_CLK_DISABLE();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
HAL_RCC_DeInit();
HAL_DeInit();
__disable_irq();
SCB->VTOR = APPLICATION_BASE_ADDR;
/* let's do The Jump! */
__set_MSP(*(__IO uint32_t*)APPLICATION_BASE_ADDR);
Jump();
}
Both of codes are generated with STM32CubeMX. Both main.c code are:
Bootloader
int main(void){
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART3_UART_Init();
while (1) { }
}
Application
int main(void){
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART3_UART_Init();
while (1){
HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin);
HAL_Delay(500);
}
}
I also modified linker files as shown:
Bootloader
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x08000000;
define symbol __ICFEDIT_region_ROM_end__ = 0x0807FFFF;
define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;
define symbol __ICFEDIT_region_RAM_end__ = 0x2002FFFF;
define symbol __ICFEDIT_region_CCMRAM_start__ = 0x10000000;
define symbol __ICFEDIT_region_CCMRAM_end__ = 0x1000FFFF;
Application
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x08080000;
define symbol __ICFEDIT_region_ROM_end__ = 0x081FFFFF;
define symbol __ICFEDIT_region_RAM_start__ = 0x20000000;
define symbol __ICFEDIT_region_RAM_end__ = 0x2002FFFF;
define symbol __ICFEDIT_region_CCMRAM_start__ = 0x10000000;
define symbol __ICFEDIT_region_CCMRAM_end__ = 0x1000FFFF;
When I try to debug bootloader code, so I push the button, the led should toggle in my application only lights up. If I try to stop debug, it seems the jump is correctly done. So where is the problem? Could you help me please? Thank you.
Best regards,
Antonio