LittleFS problem in mounting STM32L4xx (SOS)
Microcontroller : STM32L476RG,
External flash : AT45DB041E (4Mbit, 256 bytes of page, 2048 bytes of block),
SPI2 communication protocol, using HAL.
I am not able to use the LittleFS library in order to read a file that is written into the flash or any way I cannot even mount the flash. Every time I am getting the same error : (LFS_ERR_CORRUPT and after format it returns LFS_ERR_NOSPC, which is No space left on device). I don't know what it the problem I have configured some function based on the datasheet of the external flash in order to read, write and erase. I have imported the 4 basic files for littlefs into STM32CubeIDE and I don't know how to configure the cfg properly. My approach is this:
/***** LittleFS functions *****/
int block_device_read(const struct lfs_config *c, lfs_block_t block, lfs_off_t off, void *buffer, lfs_size_t size)
{
/*Find the physical address*/
uint32_t address = (block * c->block_size) + off + FLASH_BASE;
/*Perform an array read*/
// at45db_read_buffer(address, 0, size, buffer);
buffer_read(1, address, (uint8_t *)buffer);
return 0;
}
int block_device_prog(const struct lfs_config *c, lfs_block_t block, lfs_off_t off, const void *buffer, lfs_size_t size)
{
/*Find the physical address*/
uint8_t address = (block * c->block_size) + off + FLASH_BASE;
/*Transmit data to flash memory through buffer 1*/
at45db_load_data_into_buffer(1, address, size, (uint8_t *) buffer);
return 0;
}
int block_device_erase(const struct lfs_config *c, lfs_block_t block)
{
/*Find the physical address*/
uint32_t physical_address = (block * c->block_size) + FLASH_BASE;
/*Erase the block*/
uint16_t res = at45db_block_erase(physical_address);
if (res == 1) {
/*Success*/
return LFS_ERR_OK;
} else {
/*False*/
return 1;
}
}
int block_device_sync(const struct lfs_config *c)
{
return 0;
}
lfs_t lfs;
lfs_file_t file;
uint8_t lfs_read_buf[256];
uint8_t lfs_prog_buf[256];
uint8_t lfs_lookahead_buf[32]; //256/8
uint8_t lfs_file_buf[256];
const struct lfs_config cfg = {
.read = block_device_read,
.prog = block_device_prog,
.erase = block_device_erase,
.sync = block_device_sync,
// block device configuration
.read_size = 256,
.prog_size = 256,
.block_size = 2048,
.block_count = 256,
.lookahead_size = 16384,
.cache_size = 2048,
.block_cycles = 500
.read_buffer = lfs_read_buf,
.prog_buffer = lfs_prog_buf,
.lookahead_buffer = lfs_lookahead_buf,
};
/*Mount the external flash memory*/
short err = lfs_mount(&lfs, &cfg);
/**
* Reformat if we can't mount the file system.
* This should only happen on the first boot.
* */
if (err) {
err = lfs_format(&lfs, &cfg);
err = lfs_mount(&lfs, &cfg);
}
The function for reading/writing/erasing are correct, since I test with some dummy data to see if I can write the external flash, read it and erase it as well. All works fine. What is wrong here? The think is that I can't use FatFS because the file that is written into the external flash is based on LittleFS.
Question:
Is this the proper way to tell the LFS to mount the external flash? Or it is trying to mount the internal flash and it sees wrong configurations and it crashes?