Question
Looking for closest software example for implementing Dual Role Power UFP port. According to specification, such port should identify as power sink during initialization, and (in our application) after initialization perform a power role swap comman
Question 1: are there any benefits to using standalone PD controller like STSUB1600 over integrated solution STM32G0x1
Question 2: are there code examples that are reasonably close to the DRP functionality ? In all the X-CUBE-USB-PD examples I've seen it's very hard to follow the logic through all the boilerplate code, and not clear when is required to simply initialize the port.