Skip to main content
Visitor II
September 28, 2023
Solved

Lora Sx1262 integration

  • September 28, 2023
  • 3 replies
  • 7080 views

Hey,

I want to Integrate with Lora module sx162 with stm32  Board. Can any one Help me ??

    This topic has been closed for replies.
    Best answer by Issamos

    Hello @VDodi.1 

    I think you should use this drive. But I suggest you to use one of the STM32WL MCUs who combine an STM32WL and an sx126x in the same MCU. It has also a firmware that will make it easy to use (configuration, exemples,....).

    Best regards.

    II

    3 replies

    VDodi.1Author
    Visitor II
    September 28, 2023

    its Lora 1262.

    IssamosAnswer
    Graduate II
    September 28, 2023

    Hello @VDodi.1 

    I think you should use this drive. But I suggest you to use one of the STM32WL MCUs who combine an STM32WL and an sx126x in the same MCU. It has also a firmware that will make it easy to use (configuration, exemples,....).

    Best regards.

    II

    VDodi.1Author
    Visitor II
    October 7, 2023

    I don't Find any spi call function ??

     

    Graduate II
    September 28, 2023

    Perhaps look at reference schematics and Arduino shields to understand the circuit and connectivity expectations. 

    Visitor II
    September 8, 2025

    Hi @Tesla DeLorean,This is ANTONY can you help me to this, I have customised board, I want to connect with the LoRaWAN for uplink and downlink, I have using STM32F103C8T6 MCU chip if you are ready can we discuss 

    Graduate II
    September 9, 2025

    Yeah, the F1 is a bit antiquated, most of the LoRa / LRWAN stuff targets the lower-power STM32 families

    https://github.com/Saba-abiri/LORA1262

    For the Cube add-ons there's https://www.st.com/en/embedded-software/i-cube-lrwan.html

    But again not explicitly targeting the F1, so you'll be responsible for doing the porting work. Not a target I'd choose, I migrated the older LRWAN/Semtech libraries, on L1, L0, F4 platforms, for P2P

    There might be some forks in Arduino using the radio libraries, but as I recollect these are more LoRa P2P

    https://community.st.com/t5/others-hardware-and-software/interfacing-sx1262-lora-module-using-spi-dma/td-p/833871