Losing RTC ticks after wakeup timer
Hi
I have a STM32L433 running at 16MHz and having a strange issue. I have setup the rtc and within the Systimer interupt I display the current time (the systimer is 1KHz and every 1000 ticks I get the second , at this point I read the clock and display on the terminal). The time is accurate , even after a few hours its still perfect. Now if I set the wakup timer to interupt every 5 seconds, it loses some ticks after the interupt. Below is a snapshot of the terminal app. Every second the time is displayed, and at the point of ****** TIMER 5 secs ****** , this is when I set the wakeup timer. As you can see it always displays the same time twice right after the timer set . After a few timer interupts, the time is a few seconds out.

My code is as follows:
1.The inisialisation routine:
void InitRTC(void)
{
if(RTC->BKP1R!=0x1954)
{
if((PWR->CR1 & PWR_CR1_DBP) ==0)
{
PWR->CR1 |= PWR_CR1_DBP;
while((PWR->CR1 & PWR_CR1_DBP)==0);
}
RCC->BDCR &= ~(RCC_BDCR_LSEON | RCC_BDCR_LSEBYP);
RCC->BDCR |= RCC_BDCR_BDRST;
RCC->BDCR &= ~RCC_BDCR_BDRST;
while((RCC->BDCR & RCC_BDCR_LSERDY)==0)
RCC->BDCR |= RCC_BDCR_LSEON;
RCC->BDCR &= ~RCC_BDCR_RTCSEL;
RCC->BDCR |= RCC_BDCR_RTCSEL_0;
RCC->BDCR |= RCC_BDCR_RTCEN;
RTC->WPR = 0xCA;
RTC->WPR = 0x53;
RTC->ISR |= RTC_ISR_INIT;
if((RTC->ISR & RTC_ISR_INITF) == 0)
RTC->ISR = (uint32_t)0xFFFFFFFFU;
while((RTC->ISR & RTC_ISR_INITF) == 0);
while((RTC->ISR & RTC_ISR_ALRAWF)==0);
RTC->PRER = 0x007F00FF;
RTC->ISR &=~ RTC_ISR_INIT;
RTC->WPR = 0xFF;
RCC->BDCR |= RCC_BDCR_RTCEN;
RTC->BKP1R=0x1954;
}
}
2. in the systimer routine, running at 1KHz
void SysTick_Handler(void)
{
static int SecCtr=0;
if(++SecCtr>=1000)
{
SecReached=1; //volatile
SecCtr=0;
}
....
}
3. Every 5 seconds the timer gets set.
////////////////////////////////////////////
//EXTI 20 RTC Wakeup Timer
void RTC_Set_TransmitSlotTimer(unsigned short int TimeSecs)
{
RTC->WPR = 0xCA;
RTC->WPR = 0x53;
RTC->CR &= ~RTC_CR_WUTE; //clear wakup timer
while ((RTC->ISR & RTC_ISR_WUTWF) != RTC_ISR_WUTWF)
;
RTC->WUTR=TimeSecs;
RTC->CR &= ~RTC_CR_WUCKSEL;
RTC->CR |= RTC_CR_WUCKSEL_2;
EXTI->RTSR1 |= EXTI_RTSR1_RT20;
EXTI->IMR1 |= EXTI_IMR1_IM20;
EXTI->EMR1 |= EXTI_EMR1_EM20;
EXTI->PR1 |= EXTI_PR1_PIF20;
RTC->CR |= RTC_CR_WUTIE;
RTC->CR |= RTC_CR_WUTE;
RTC->ISR = ~RTC_ISR_WUTF;
NVIC_EnableIRQ(RTC_WKUP_IRQn);
NVIC_SetPriority(RTC_WKUP_IRQn,6);
RTC->WPR = 0xff;
if(DebugMessage)
Debug("\r\n**** WUTF set ****\r\n");
}
4. And in the interupt routine.
void RTC_WKUP_IRQHandler(void)
{
if(RTC->ISR & RTC_ISR_WUTF)
{
FiveSecInterupt=1; //volatile char
EXTI->PR1 |= EXTI_PR1_PIF20;
}
}
5. And within the main routine.
while(1)
{
if(SecReached) //set in timer interupt.
{
ReadTime();
sprintf(ScrapBuffer," %02d:%02d.%02d\r\n",Tme.Hour,Tme.Min,Tme.Sec);
Serial_PutString(USART2,ScrapBuffer);
}
if(FiveSecInterupt) //set in wakeup interupt
{
Serial_PutString(USART2,"\r\n****** TIMER 5 secs ******\r\n");
RTC_Set_TransmitSlotTimer(5);
}
}
Can someone please let me know why I am losing clock ticks ?
Many thanks
Scott